AXIS#.ENDEFAULT

Description

AXIS#. ENDEFAULT sets the default state of the software enable on power up for axes not controlled by a fieldbus (AXIS#.CMDSOURCE other than 1). Set AXIS#.ENDEFAULT to 1, to enable an axis automatically on power-up. Set AXIS#.ENDEFAULT to 0, to have the axis disabled on power-up.

Example

Code

Queries the default state of Axis 2 on power-up:

--> AXIS2.ENDEFAULT
0

Automatically enables Axis 2 on power-up:

--> AXIS2.ENDEFAULT 1

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also AXIS#.EN | AXIS#.CMDSOURCE

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.ENDEFAULT 0x5000 0xA USINT - - RW False
AXIS2.ENDEFAULT 0x5100 0xA USINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen